Upgrade to a high-performance PC with JOY-IT’s upgrade kits

Breathe new life into your ageing PC or use it as the basis for a completely bespoke configuration. Is your computer getting on in years and the new off-the-shelf PCs on the market don’t meet your individual needs? Are you also looking for a cost-effective, environmentally friendly solution that saves you the hassle of new […]
Chat GPT – concrete applications for companies

In the first part of this series, we looked at whether ChatGPT could be used for industrial applications. And if so, what needs to be considered. Now it’s time for the application. We want to know how well the tool works in practice. We looked at three specific application areas. Text creation – amazing results, […]
ChatGPT – ready for industrial use?

The AI-based tool ChatGPT from the company OpenAI is a source of immense fascination worldwide. Almost daily, the media reports on amazing features, but also on bugs and weaknesses of the large language model. So we ask ourselves the question: Is ChatGPT suitable for industrial use? What is ChatGPT? In a few words, ChatGPT is […]
Switchgear unit and digital control construction

From conception and project planning to standardisation and optimisation measures: In the age of Industry 4.0, the profession of electrical design engineer requires a wide range of skills and tools. From digital planning or even digital production to digital documentation and maintenance, the day-to-day work of electrical engineers has changed faster than the existing tool […]
How to make an infrared remote control for your tube amp

Tube amplifiers are audio devices that are at the higher end of the price range. Despite their high price, most devices only allow operation directly on the device. There are remote controls for very few. This is where the following project comes in. Three basic functions are realized in this self-built remote control: There is […]
How to set up a Smart Mailbox

Intelligent voice assistants, washing machines or electric shutters: even though our homes have become smarter and smarter, there is still room for improvement with regard to the classic mailbox. So that you know immediately when you receive mail, you can also make your mailbox smart with a few simple steps. This How-To explains what options […]
Why data backup is so important for SMEs and the self-employed?

In a digitized world, data is the basis for far-reaching and promising business decisions. But companies can only take full advantage of these benefits if they can rely on sustainable data backup. While it is mostly annoying for private individuals when important data such as photos or similar are lost, it can be business-threatening for […]
Saving power with the four-channel remote switching system

Electronic devices run on electricity. Even when they are switched off, energy flows through the cables and out of the power grid. For example, a normal workstation may be consuming up to 100 watts of power without a device actually running. Common 433MHz remote switching systems achieve only limited success. This project shows you how […]
Ergonomically designed workplaces for more comfort

Musculoskeletal disorders, diseases of the respiratory tract or mental illnesses – these are all possible consequences of permanent stress at the workplace. Ergonomically designed workplaces can nip these complaints. This How-To explains how to align your desk according to the principles of ergonomics and what you need to keep in mind. Ergonomy Since ergonomics is […]
Tips and ideas for case modding

Gone are the days when computer cases were just a place to store hardware components. With custom lighting and other components, users can turn their cases into real works of art. Case modding is the name of the game. Modifying the hardware not only improves the look, but also the performance. Here we show you […]