Today, PCE Instruments is one of the most successful international suppliers of professional measurement technology. Customers all over the world rely on measurement solutions from PCE Instruments. PCE measuring and testing instruments offer a wide range of products, which are constantly adapted to the current requirements of the users. The main focus of PCE Instruments is on mobile measurement technology for a wide range of industries and applications in industry, research and development. The acquisition, documentation and evaluation of measurement data is becoming more and more important in all conceivable areas; with measurement solutions from PCE Instruments this can be realised quickly, precisely and easily.
PCE Instruments offers complete solutions for demanding, industrial and modern measurement tasks. Maximum reliability in all inspection and non-destructive testing measurements is ensured by a wide range of measuring instruments that determine and analyse the quality of various scientific and industrial applications without damaging the material.
If there are deviations from the previous values in various manufacturing processes, the manufacturing costs would increase and there would also be a loss of time. PCE Instruments offers preventive solutions that can detect possible deviations directly in the production process, thus reducing both costs and downtime.
The ultrasonic flow meter

A flow meter is used to determine the velocity and, under certain conditions, the volume of a flowing fluid. Flowmeters can be classified according to the type of fluid being measured and the principle of measurement. Often the flow meter is designed for a specific type of fluid, i.e. it measures either gases or liquids. Specially equipped units can even measure bulk materials that are free flowing during transport, manufacturing or storage processes.
Temperature measurement
Temperature instruments for surface, gas and liquid measurements, contact or non-contact.
PCE Instruments’ temperature measurement products offer quality and value for money. Many testers store the measured values, some transfer the data to other devices such as smartphones or PCs, so that they can be processed directly.
PCE Instruments offers a wide range of temperature measuring instruments for industry, trade and research, from penetration thermometers to 12-channel data loggers and thermal imaging cameras.
Condition monitoring

The key word in industry is downtime. And it is precisely this downtime that needs to be minimised. One tool for this is continuous condition monitoring (automated or manual).
More precisely, the task is to stop industrial systems (to maintain the condition of the machines) only at the desired time, according to plan, and to restart them smoothly. Maintenance and repair work can be carried out during the planned downtime.
Non-destructive testing
Non-destructive testing (NDT) plays an important role in the analysis of structural and mechanical components in the maintenance and repair of machinery and equipment.
The safe and long-term stable use of the components is crucial and therefore they should be subjected to non-destructive testing. PCE Instruments offers various measurement categories for non-destructive testing, including visual inspection, ultrasonic testing and leak testing.
These methods ensure reliable inspection of components without damaging or affecting them.
Industrial weighing technology
In the field of industrial weighing technology, PCE Instruments offers scales for recording the masses of raw materials in incoming goods inspection, for checking stock levels, for dosing components or for determining masses in various stages of the production process.
Whether in the food industry, pharmaceutical production, chemistry, retail or scientific laboratories, the correct use of weighing technology not only ensures the quality and safety of products and experiments, but is also crucial to the efficiency of processes and research work.
PCE Instruments offers a wide range of scales with different performance and features, from moisture analysers to parcel scales to drive-through scales.
Temperature and humidity measurement
Temperature and humidity measurement for warehouses or for use in air conditioning and ventilation systems and ductwork.
Whether raw materials, auxiliary materials, semi-finished or finished goods are stored, climate measurement is usually required. PCE Instruments offers humidity measurement systems that are delivered pre-configured and can be installed quickly and easily.
Gas measurement technology
When it comes to gas detection, the safety and protection of people, the environment and property are paramount.
Whether portable gas detectors for mobile use or stationary gas warning systems, PCE Instruments offers options for personal protection and the safety of machines, plants, goods and raw materials with both standard products and customised gas measurement technology.
Environmental and climate measurement technology
Environmental and climate measurement technology plays a vital role in environmental protection and climate change research, as well as in the production of food and drinking water.
Accurate measurement and analysis of environmental parameters and climate change enables better informed decisions to be made to protect ecosystems, improve air and water quality and mitigate climate change.
The PCE Instruments portfolio includes a wide range of environmental instruments that collect valuable data for these purposes, from anemometers to temperature meters to pollution monitors.

Images: PCE Instruments