Do you know a business that can do without a reliable, high performance storage solution? Not us. SYNOLOGY has developed a versatile and intelligent NAS that stores all company data in a central location and is expandable. With minimal configuration, the DiskStation DS923+ offers a comprehensive range of easy-to-use applications for file management, multimedia organisation and data backup. It also protects you from cyber threats. This compact storage solution is ideal for IT professionals, creative professionals and businesses.
Versatile for a wide range of needs
Businesses in a wide range of industries can attest to the fact that slow work processes affect productivity and lengthen project timescales. Slow data processing can lead to a loss of competitiveness. And customer satisfaction depends on the availability of services and content. For all these challenges and more, the DiskStation DS923+ provides a central and highly scalable storage location. The storage solution has four slots and a base capacity of 50TB. This next-generation NAS delivers lightning-fast data sharing, smooth synchronisation, seamless streaming and reliable backup for multiple users. In numbers, this means sequential reads of up to 625MB/s and sequential writes of 559MB/s.
A generous 32GB of RAM ensures that the internal system remains stable and protected from potential crashes. Automatic data error correction ensures that data errors are automatically detected and repaired. For the company, this means time-saving, accurate and cost-effective data management, ensuring smooth internal processes as well as external partners and customers. The two Gigabit RJ-45 ports can be interconnected using Link Aggregation to provide automatic network failover and load balancing for robust network performance.
The NAS grows with your business! If you need even more storage, upgrading is a breeze. With the DX517 expansion, you can increase capacity to over 120TB with up to nine drives. There are also slots for faster storage devices (2x NVMe SSDs) to further boost performance. For an even faster internet connection, a network enhancement module can be added to achieve 10 Gigabits per second.
Exciting use cases in your organisation
The DS923+ is a powerful solution for many scenarios where secure and flexible storage is required.

Safe storage for many years
All businesses, regardless of size, need to keep all their company-related tax records in a secure location for an extended period of time. The NAS allows you to organise and store your financial records in a compliant manner. It also means you are prepared for a possible tax audit.

Virtual Machines and Containers
The server solution offers extensive options for virtualisation requirements and can be configured as certified storage. For example, you can set up your virtual machines (VMs) on the NAS by allowing VM data to be stored. Of course, the Disk Station can also be used as a backup server for VMs to protect sensitive data. It can also host lightweight containers and VMs for flexible and efficient deployment of applications and services.
Monitoring in a protected environment

Most businesses use cameras to protect themselves against intruders, for example. When it comes to storing surveillance video, privacy and legal requirements need to be taken into account. This is why you can also integrate surveillance functions into your central data hub. These work on the basis of event-based rules that you define in advance. Video can then be encrypted and stored in a secure, private location of your choice. You can access it from anywhere, at any time, via browser or app.
Private Cloud Solution Features, Applications and Functions

Privacy and data security for your business
A private cloud gives you complete control over your own data and where it is stored. This means that as an organisation, you can remain GDPR compliant and prevent data from being stored in countries that do not comply with local data protection regulations. Your company’s data can be expertly protected and managed using the intuitive SYNOLOGY DSM operating system, which is based on the advanced Btrfs file system. Features such as scheduled snapshots, file and folder recovery, flexible storage quota management and file self-healing help detect and recover damaged files.
In addition, inline compression reduces storage consumption and extends drive life by compressing data before storing it. SYNOLOGY DSM integrates multi-level backup with its NAS at no extra cost. The Active Backup Suite ensures fast recovery of various devices and SaaS applications.
Other features of the backup solution include snapshot replication to protect against unwanted changes or ransomware attacks. Hyper Backup provides efficient backup and version management, while C2 Storage gives you access to secure storage in public clouds.
Effective tools for successful teamwork
The following applications and features make team collaboration more successful and productive. In SYNOLOGY’s NAS-accessible Productivity Suite, all employees in different locations can simultaneously edit documents, share files, manage emails and send instant messages, among other things. SYNOLOGY Drive acts as a cross-platform synchronisation server, allowing you to collaboratively edit and manage files and create secure links for data sharing. Integrated with Drive, SYNOLOGY Office Extension enables real-time collaboration on password-protected documents. This includes the ability to view and manage changes through version tracking. Visual assets can be shared with project stakeholders using the privacy-focused sharing options in SYNOLOGY Photos. And SYNOLOGY Hybrid Share combines reliable local storage with efficient synchronisation of shared folders in the cloud.
The SYNOLOGY DiskStation DS923+ is now available in the reichelt online shop.
Images: Adobe Stock, Synology