Intuitive technology and ease of use
At the heart of MiniBrew is an intuitive app in English, available for iOS and Android. It provides detailed instructions for the entire brewing process. Videos and pictures explain every step, from brewing to fermentation, which takes 10 to 36 days depending on the type of beer. When the beer is ready to drink, the app notifies the user. This means you can enjoy fresh beer straight from the keg at any time.

Another advantage of the MiniBrew is the fully automatic cleaning process. Anyone who has ever brewed their own beer knows how time-consuming cleaning is. MiniBrew makes this easier by cleaning the system automatically, saving you time and effort.
Personalised beer creations and access to exclusive recipes
The basic package includes a SmartKeg and a complete set of utensils. With the separately available kegs, multiple beers can be brewed and tapped at the same time with MiniBrew. Users can experiment with different yeasts, hops and other ingredients to create their own beer creations. A large selection of brewing kits also makes it possible to brew popular beers without experimenting.Paid access to the MiniBrew community opens the door to more than 10,000 beer recipes. From Kölsch to Imperial Stout, Tripel to Porter, the selection is impressive and will make any beer fan’s heart beat faster. Access allows users to monitor and programme their brewing creations, making the brewing experience both flexible and user-friendly.

In short, MiniBrew is more than just a brewer. It is a complete brewing system that will fundamentally change the way we brew beer at home. It promises a future where beer lovers can live their passion to the full, supported by technology that is as practical as it is innovative. MiniBrew is brewing with intelligence.
Images: MiniBrew