The Raspberry Pi Zero WH is now available online from reichelt.
The Raspberry Pi provides concentrated power in a handy, compact format, enabling countless possibilities for creative projects. The Raspberry Pi Zero WH is the minimalistic model for those who need an efficient development board, but not full computing power or as many connectors. Find out more about the features of the mini-board below.
Compact format, compact performance
The Raspberry Pi Zero WH is the smallest developer board with a GPIO bar of just 6.5cm by 3cm. The computing power of the single-core processor comes to 1 GHz and the RAM has 512 MB. The connections are also significantly reduced but are available in mini format, such as the mini HDMI socket or the micro USB power supply. So, when buying a board, it pays to think about whether you need an adapter.
The mini Raspberry Pi has several advantages compared to the original Zero model. The Zero WH comes with integrated WLAN and also has Bluetooth and a camera connection.
Specifications:
- 1GHz single-core CPU
- 512 MB of RAM
- Integrated WLAN (802.11b / g / n)
- Mini HDMI port
- Micro USB OTG port
- Power supply via micro USB
- Micro-SD
- 40 pins (HAT compatible)
- Bluetooth 4.1
- CSI and audio jack
Perfect for creating a smart home
The biggest advantage of the Raspberry Pi Zero WH is its low power consumption. Ideally, it only needs 90 mA and up to 230 mA under working conditions (the bigger boards are often need more). This makes it particularly good for applications that will be running for a long time, but do not have to perform particularly complex or intensive tasks, such as a temperature meter or motion detector.
With its compact size, low power consumption and integrated WiFi, the Raspberry Pi Zero WH is the ideal board to create smart home devices.
Image: reichelt