The HKTDC Hong Kong Electronics Fair and the Global Sources Consumer Electronics Trade Show are two of the world’s largest and most important international trade fairs for electronic products and services. They take place in Hong Kong and offer a wide range of products, including many trends and innovations.
We continued to be there in the spring to keep abreast of trends and innovations in consumer electronics, industrial electronics, information technology, telecommunications and consumer electronics so that we can constantly develop our range of products and services for you. Profit from this modern offer at a top price-performance ratio – based on long-standing business relationships.
GaN- and AI-based technologies at a fair price
One of the latest technology trends in the field of charging technology is gallium nitride (GaN). So far, the most common semiconductor material in power supplies is still silicon. However, the technological development of Si power supplies has reached its limits in recent years. The use of gallium nitride makes larger further developments possible again and offers higher performance with lower space requirements.Compared to silicon, gallium nitride has the advantage that not as many components have to be installed as with conventional Si power supplies. This means that power supply units can be built much more compactly. At the same time, GaN has a higher bandgap efficiency. For this reason, current can be conducted through a gallium nitride chip much faster than through silicon. This makes the effective use of new connection technologies, such as USB-C, possible. Your advantage: you can charge your compatible devices significantly faster than with a standard USB-A connection.
The increased efficiency also has the advantage that less heat is generated during the current flow and the few necessary components can be installed even closer together. Thus, a higher power density is possible, as with our new 100 W USB-C power supply.
It is not only universally applicable for all USB devices with USB-A and USB-C, but also offers up to 100 W of power thanks to PowerDelivery. This enables fast charging of current smartphones and tablets and even notebooks and MacBooks. To ensure that the charging process is not only fast but also safe, the power supply has integrated protections against excessive current flow, overcharging and overheating.
Artificial intelligence (AI) has become a major technical innovation worldwide. The performance of current AIs opens up previously unimagined fields of application for machine learning. The NVIDIA® Jetson Nano™, especially for edge computing, deserves a special mention. It delivers up to 472 GFLOPS of accelerated computing power, can run many modern neural networks in parallel, and has the power to process data from multiple high-resolution sensors – a requirement for full AI systems.The Jetson Nano is powered by NVIDIA JetPack™, which includes a Board Support Package (BSP), Linux OS, NVIDIA CUDA®, cuDNN, and TensorRT™ software libraries for deep learning, computer vision, GPU computing, multimedia processing, and more offers. It is also production-ready and supports all major AI frameworks.
This makes the Jetson Nano the ideal platform for the development of mass-market AI products such as AIoT gateways, intelligent network video recorders and cameras, consumer robots and optical inspection systems.
Our bundle makes it easy for you to enter the AI world or expand your existing systems. The NVIDIA® Jetson Nano™ bundle from seeed contains the NVIDIA® Jetson Nano™ module, the NVIDIA® Jetson Nano™ carrier board, matching heatsinks, a robust housing and the pre-installed JetPack software. So you can start developing your IoT solutions straight away.
Quality of products and safety standards
All products that we intend to include in our range directly from the trade fairs in Hong Kong are checked by our in-house technicians for conformity with the defined quality standards and specifications. This means that you will always benefit from a modern range of products of excellent quality and will be able to successfully and satisfactorily implement your projects with us.To support you in this, we have already included many inexpensive and powerful measuring devices from Uni-Trend in our range in recent years. Among them is the high-quality, industrial all-round multimeter UT 161D.
The robust and reliable multimeter is suitable for use in a wide range of environments. It is particularly suitable for industrial use, but also has a wide range of functions that can be used in research, education and school environments. Ambitious home users will also appreciate the measuring device thanks to its simple operation.
The multimeter scores with
- a large and illuminated display for quick reading of the measured values
- Auto-range function and 6,000 counts for precise measurements
- extended features, such as temperature measurement + LoZ ACV
- as well as a USB connection that makes it possible to evaluate the measurement results on a PC.
Conclusion
Put your projects on the fast track with the latest technological developments we have carefully selected for you, giving you a competitive edge at the top price. In the future, we will continue to be on site for you in Hong Kong to discover the next innovations. That’s why reichelt is “The best part of your project”.
Images: Adobe Stock, reichelt elektronik