The perfect indoor garden for cooking fans with a green thumb: with Véritable’s kitchen gardens you can grow two or four different plants in parallel and harvest them weekly for up to six months.
Fresh herbs all year round
The Véritable kitchen gardens are designed for indoor use. The design is both functional and visually appealing. Thanks to its compact size, the miniature garden will find a suitable place in any kitchen. This is an attractive option, especially for city dwellers, who can process fresh herbs or vegetables regardless of the current season.
The construction and commissioning of the kitchen garden is simple, fast and user-friendly: the garden is connected to the power supply via a plug, the water reservoirs are filled and the culture media are inserted. Three weeks later, the first herbs can be harvested.
Healthy freshness from own cultivation
Rich nutrient media as well as biological, GMO-free seeds are already supplied. The prospective kitchen gardener can choose between a variety of local and exotic herbs, young vegetables such as tomatoes or peppers, berries and edible flowers such as courgette blossoms. So there is always something healthy and fresh on your plate – even in the deepest winter.
Thanks to smart technology: rich harvest at low cost
The LED lamps ensure that the day/night cycle is as natural as possible, so that the plants get enough light regardless of their location. Light sensors also ensure that the lamps are geared to the natural lighting conditions on site. This gives the plants the right intensity of lighting and ideal conditions for good growth.The smart irrigation system can be operated manually or through the Véritable App with Classic, Smart or Connect technologies. It also works autonomously for up to four weeks – a big plus for busy and professional travellers.
Thanks to in-depth research and development ideally tailored to the needs of the plants, the Véritable Kitchen Garden guarantees the best conditions for the kitchen plants in terms of size, irrigation, light and pH. This enables it to regularly produce fresh herbs, vegetables and more – directly from the kitchen garden to the plate.
Picture source: AdobeStock/125818014